AXIS#.SAFEPARAM.SBT.MAXAPPLOAD

Description

Specifies the maximum load of the application reflected to the motor shaft converted to current in mA. This value is scalar without regard to direction. It defines the 100% maximum application load. The Safe Brake Test (SBT) is done with 130% of maximum load (current).

 

Parameters Editor with the Max Application Load row circled

Context

For complete SBT information refer to SBT (Safe Brake Test).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

02-01-02-000

General Information

Type

Read/Write

Units

mA

Range

1 – 200000 mA

Default Value

1000 mA (1 amp)

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SBT.MAXAPPLOAD

3157h

03h

Unsigned32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SBT.MAXAPPLOAD

3257h

03h

Unsigned32

-

-

Read/Write

No